Email Address:
 
Password:
 
PBC Linear Company Logo
LINEAR MOTION SOLUTIONS
TOLL-FREE 1-800-962-8979
 
Zach Olsen

In today’s world of space conservative technology – flat-screen TV’s, 1’’ thick laptops and smart phones – the demand for printed circuit boards is on the rise. Assembling printed circuit boards requires repeatable performance and extremely subtle precision is usually too expensive for educational and small business markets. Professor Harvey Silverman’s team at Brown University has recently devised a solution to automate the process using PBC Linear’s ML series mini-actuators in a multi-axis circuit board assembly system at a suitable cost for these areas.PCB Assembly Graphic

To accomplish the task of circuit board assembly, Professor Silverman needed a linear motion solution that could position tiny surface mount devices (SMD’s) such as capacitors and resistors of 0402 size (0.040’’ x 0.0240’’) and accurately place them onto solder paste to adhere to the board. The tiny parts need to be handled delicately and adjusted mid-operation to correct for misalignment. The final piece of the puzzle was finding a way to ensure all parts are in the right place.

An ML series XYZ gantry controlled with a vision system was the perfect solution. With a 28 x 32 mm profile, the compact mini-actuator was the optimal size for small-scale circuit board assembly. Also, the ML series is equipped with state-of-the-art components for accurate linear positioning; such as a ‘dove-tail’ style carriage comprising 14 plane bearing surfaces for high rigidity and smooth travel, single or dual external linear guide supports for enhanced stability and a full line of accessories for use in multi-axis systems.

Designed over the course of a year with product assistance from expert PBC Linear application engineers, Professor Silverman came up with a working solution. Three PBC Linear ML series mini-actuators assembled in a 12 x 14’’ footprint XYZ system were utilized to automate the surface mount assembly process. Two ML actuators accurately determine XY position while the third moves a vacuum needle part-grabber up and down. A server was also added to allow rotation of the part. In addition, the gripper assembly is outfitted with a small camera to locate loose parts and give feedback to the user utilizing software designed by Ken Silverman. The camera compares images of assembled circuit boards to identify where all the pieces need to go and signals the gripper to re-align if adjustment is necessary. The system can also be switched over to manual control for special assembly projects.

Overall, Professor Silverman was very pleased with the low cost PBC Linear ML solution and its ability to perform the required tasks at hand. He is currently working with PBC Linear engineers to update the design with a new ML series actuator for enhanced pick-and-place assembly. For more information on the ML series or any other PBC Linear actuator solutions, such as more application examples and detailed technical data, please call 1.800.729.9085, email to marketing@pbclinear.com or visit us at our LAT dedicated webpage at LAT.pbclinear.com.
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
Site Map | Contact Us | Terms & Conditions | Purchase Order Terms | Privacy Statement | Return Goods Policy | ROHS Certification | India Steel | Conflict Minerals