Email Address:
 
Password:
 
PBC Linear Company Logo
LINEAR MOTION SOLUTIONS
TOLL-FREE 1-888-389-6266
 
Zach Olsen

ML Linear Actuators Named as Design News Best Product Finalist

September 04, 2009 - Rockford, IL  -  Posted by Zach Olson

Golden Mousetrap Award Finalist for Motion Control by Design News 

PBC Linear’s ML series miniature linear actuator has been named a finalist for the Golden Mousetrap Best Product Award in Motion Control! Officially announced in the September 2009 issue of Design News, the Golden Mousetrap awards the year’s top products in innovation, creativity and product design. After a record number of entries in each of the four different categories—Electronics, Motion Control/Automation, Hardware/Software, Material Fastening—73 finalists and 23 winners were selected as the leaders.

Founded in 1946, Design News is a leading technical resource for design engineers specializing in a range of different fields. Design News began the Golden Mousetrap Awards two decades ago, focusing on products that bring new ideas and innovation to the engineering world. The products are judged by a panel of experts in that particular technical field. PBC Linear was named a finalist last year in motion control for their cost effective linear guide technology, Integral V™. This year, PBC Linear introduced their new line of miniature actuators, the ML series.

Golden 
Mousetrap Award

Incredible precision and performance delivered in a compact profile, the ML series is the perfect solution to small-scale linear motion. With the entire system measuring only 28 x 32 mm—varying lengths available—the ML series can be installed into almost any system. The outer profile is post-process precision machined to ensure exact mounting and high accuracy travel. Available in several different design options, the ML series can support dual external linear guides to enhance stability and load capacity; the ML also features a wide variety of lead screw sizes to optimize the actuation speed. Other customizable options include flexible motor mounting, a seal strip to restrict contamination and a full selection of state-of-the-art stepper and servo motors. Combining all of the features that fully adapt to the customers’ specific needs with expert engineering design, the ML series mini-actuator excels in several industries; including lab automation, medical, bio-tech and all compact linear positioning applications. 

For more information on the ML series, please call 1.800.729.9085, email to marketing@pbclinear.com 

Learn more about our ML Miniature Linear Actuator at:
www.pbclinear.com/ML-Actuators

 
 

 

blog comments powered by Disqus

Blog Posts:
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
Site Map | Contact Us | Terms & Conditions | Purchase Order Terms | Privacy Statement | Return Goods Policy | ROHS Certification | India Steel