Email Address:
PBC Linear Company Logo
TOLL-FREE 1-800-962-8979
Mark Huebner

SPS Parma - Italy 2015

The SPS show in Parma, Italy began the week of May 11, 2015 with a flurry of action today at the International Power Components (IPC) booth as crowds gathered around the 3DP1000 large format 3D printer from 3DP Unlimited that utilizes PBC Linear's industrial strength SIMO Series linear guides.  Paired with high performance stepper motors from Applied Motion Products, the 1m x 1m x 0.5m build platform 3D printer is an outstanding demonstration of complete Mechatronics Enabled automation. 

SPS Parma - 2015

The SIMO Series linear guides shown at SPS utilize the Cam Roller Technology (CRT) bearing solution that has PBC Linear’s patented preload adjustment feature built into the carriage.  This, combined with the patented anti-backlash Constant Force lead screw nut, provides the high performance required to enable the 3D printer to reach layer resolutions as low as 70-microns.

SPS Parma continues both Wednesday, May 13 and Thursday, May 14, 2015 from 09:30 to 18:00 both days at the Fiere di Parma.  Be sure to visit the IPC booth in Hall 3, Stand F002 where you can see the SIMO Series linear motion platform in action.
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
Site Map | Contact Us | Terms & Conditions | Purchase Order Terms | Privacy Statement | Return Goods Policy | ROHS Certification | India Steel | Conflict Minerals