Where does PBC Linear’s
Simplicity® technology fit into the automotive industry? Everywhere!
Testing, product feeding conveyors, assembly lines, wash down machines,
painting lines, welding applications and die storage are all examples of
applications where PBC Linear’s Simplicity® technology has been
installed and found long-lasting success providing smooth and quiet
linear motion. With a range of different factors that can effect
production in the automotive industry, having dependable linear motion
is a must. Since their first inception, PBC Linear’s Simplicity®
technology has been a long-time provider of smooth, reliable, low cost,
quiet linear motion in the automotive environment.
Metal particulate, dirt, extreme
temperatures, high shock loads, vibration, and caustic chemicals are
constant obstacles for effective linear motion in the automotive world.
From welding applications to assembly line conveyors to part washers,
linear motion products are under constant bombardment from the hazardous
surroundings. Conventional linear ball bearing systems cannot last.
Whether because of corrosion of the shaft, seizing of the ball bearing
track, or ball-bearing spalling, the filthy environment holds no place
for undependable ball bearing technology. Ball bearing use results in a
halted production line causing unplanned downtime and dramatically
increased production costs.
PBC Linear’s Simplicity® bearing comes
equipped for the job. Backed by its FrelonGold® liner, the Simplicity®
bearing is designed to last in the worst possible environments with
minimal lubrication and maintenance. This liner allows for the bearing
to handle loads up to 20x that of the competing linear ball bearing
system and increases its speed capabilities by 50%. The
Simplicity® bearing is also corrosion resistant, can handle temperatures
from -400°F to +400°F, and is virtually impervious to shock vibration.
With no moving parts to stall, PBC Linear’s Simplicity® bearings will
NOT catastrophically fail!