Bearing and linear guide manufacturers’ misuse of performance buzzwords such as “self-lubrication”, “maintenance free”, and “lubed for life” has led to a broad misunderstanding of what these terms actually mean. This confusion can lead to misapplication of products resulting in failures, downtime, and bottom line losses in productivity and dollars.
One of the most common methods used is to add a piece of oil/grease soak porous material (typically felt or plastic) to a bearing or linear guide.
Oil impregnated plastic and felt wicks may extend the life of a bearing system but they cannot be classified as “self-lubricating”. They require maintenance attention to oil levels that dissipate, age, and become ineffective over time. True “lube for life” requires that the lubrication be an integral element of the original bearing material and that no additional lubrication will be required at any point in the future, regardless of time between lubrications. To be truly self-lubricating, the lubrication cannot be an add-on, does not break down, and remains a part of the bearings makeup for its entire life without the need for outside maintenance.
What is Self-Lubricating?
Self-lubrication is characterized by the bearings ability to transfer microscopic amounts of material to the mating surface. This transfer process creates a film that provides lubrication and reduces friction over the length of the rail or shaft.
Transfer Process
The transfer process is an ongoing dynamic function of the self-lubricating bearing that will continue throughout its operational life.
The first and most critical step in the process is the break-in period. This is when the initial transfer of material to the mating surface takes place. The amount of bearing material affected during the transfer is dependent upon multiple factors including the speed, load, and length of stroke, etc. for the application. Typically the initial transfer process will be accomplished in 50-100 strokes of continuous operation.
The secondary and ongoing phase of the transfer is where the self-lubrication is most effective.
Common Misconceptions
Clever advertising gimmicks and inaccurate training materials are claiming “self-lubricating” or “lubed for life” capabilities for systems or components that do not fit the definition of the lubrication being an integral element of the bearing material. While these systems may be temporarily “self-lubricating”, the lubricant will eventually be used and need to be replaced. Many “lubed for life” bearings are not really lubed for life, they are simply “lubed for a long time”. Below is a description of some of these types of systems.
Types of Non Self-Lubricating Systems
Rolling Element Systems
These include rotary (ball and roller) bearings, round-way linear ball bearings, and rolling element profile type monorail designs. All of these systems require some kind of external lubrication to operate. The metal-to-metal contact of the rolling element against the raceway necessitates that there be grease or oil present at all times. If this external lubricant is not present, the ball or roller will begin to make direct contact with the shaft or rail material resulting in galling and brinelling damage. Many manufacturers attempt to overcome this weakness in the design by adding oil-impregnated seals to the ends of the bearing or housing. This approach can result in some benefit to the life a rolling element bearing.
Oil impregnated bronze
Bronze bearings are very porous and have lightweight oil soaked into the material. Under the optimum conditions, this oil is drawn to the bearing surface creating a lubricated layer between the bearing and the shaft.
Graphite plugged bronze
Graphite is a good solid lubricant that is normally added to a bronze type bearing. Solid plugs of graphite are usually inserted into holes in the base bronze material.
Teflon coated materials
PTFE can be used to coat bearing surfaces in several ways. It can be applied as either a part of a powder simply dusting the bearing. It can be a sprayed mixture that adheres to the bearing surface. Or it can be part of a liquid or grease compound applied to the bearing. Any of these methods results in a very thin layer of actual lubricant that is quickly worn away and becomes ineffective.
Oil impregnated plastic
Here again, lightweight oil is added to the base material to aid in bearing lubrication. The result is decreased friction initially, but lubricant aging and dissipation quickly reduce its effectiveness.
What makes a system self-lubricating?
1. The lubrication is an integral component of the bearing material.
2. The lubrication (typically oil or grease) is NOT added to the original bearing design.
3. The lubrication will NOT breakdown and be ineffective over time (lubricant aging).
4. The lubrication is consistently applied to the shaft surface.
5. Additional components do not add cost to the overall system.
To truly be self-lubricating, a bearing system must do exactly what the name implies. It must provide its own lubrication throughout the life of the system and not have some external source facilitating lubrication for a period of time. It must be designed and manufactured into the bearing material from the beginning. One example of this is PBC Linear’s Simplicity® self-lubricating liner.
The Advantages of Simplicity’s Frelon GOLD® Liner
- No metal-to-metal contact
- No galling or brinelling
- No catastrophic failure
- No added lubricants to attract additional contaminants
- Vibration dampening for smooth and quiet operation
- Actual “maintenance free” operation
Proven Success in PBC Linear™ Products
- Simplicity Linear Plain Bearings
- Uni-Guide™ Modular Guides & System
- Mini-Rail® Miniature Linear guide
Summary
The term “self-lubricating” should not evoke a generalized meaning that passively represents a broad range of different technologies striving for the same outcome. Self-lubricating refers to a specific performance advantage made possible by a unique product design that satisfies all aforementioned criteria: internal lubrication system, no added grease or oils (no maintenance), no lubrication breakdown and no added cost. In other words, “self-lubricating” must ensure the permanent, maintenance-free operation in even the most challenging environments. Designers need to learn to recognize the difference between the various types of lubrication options. Failure to do so will result in costly misapplications and re-designs.