PBC Linear's New Profile Rail Technology
Provides Long-Lasting Rigid and Precise Linear Motion

PBC Linear is proud to introduce a newly offered technology to their portfolio of linear motion products: Profile Rail Technology (PRT). Excelling in high load capacity, smooth and quiet linear guidance, PRT can be implemented in a wide range of different industries and applications

The PRT line features of a series of industry interchangeable fully sealed Linear Guides, supported by re-circulating ball bearing technology. The Linear Guides consist of carriage/runner blocks that travel along a ground hardened profile rail. The matching precision ground profiles on the rail and runner block optimize load and rigidity for ensured stability in linear motion. They also feature a new internal lubrication system that reduces periodic maintainance and expensive lubrication systems.

An optional new ball cage design dramatically reduces noise, friction and vibration and improves load capacity in the same envelope. The ball cage also features reservoirs that provide timely and even distribution of lubrication to the Linear Guide system.

       Profile Rail
       Linear Guide Catalog
    
 
Profile Rail Linear Guide Technology utilizes re-circulating ball bearing technology, high precision and long-lasting caged and non-caged runner block linear guides providing high load capacities, high speed, and years of quality linear motion. Featured with several carriage option grades, PRT can meet any application.
 

Or Call Now
For More Information
1-888-777-1497

 

With black oxide, chrome, or black chrome rail finishing for enhanced corrosion and chemical resistance, PRT Linear Guides can further extend its wear life in even the corrosive of applications. The Linear Guides are also available in a wide range of carriage/runner block designs: short, long, and extra long, wide or narrow, low or high combinations and in various degrees of precision and preloads. For sustained smooth and quiet linear motion, PBC Linear’s newly introduced Profile Rail Technology is the answer!

 

Machine tool precision at linear ball bearing prices

 

Using re-circulating ball bearing technology, high precision and long-lasting caged and non-caged Linear Guides provide low friction, high load capacities, rigidity, high speeds, and years of quality linear motion.

  • High rigidity and accuracy - (4) four row angular ball contact with integral double row sealing

  • Low noise and vibration - innovative polymer noise-reducing tube design

  • Multiple runner blocks - low and high profile runner block assemblies

  • Low co-efficient of friction

  • Optional Carriage - extra-long or short for compact spaces

  • Size interchangable

  • Completely Sealed at no additional cost
 
Precision Grade Runner Block Options
Application
Accuracy Grade
     
N
H
P
S
U
 

Machining center

 
 
 
  Lathe
 
 
 
  Milling machine
 
 
 
  Boring machine
 
 
 
  Jig borer
 
 
 
  Grinding machine
 
 
 
  Electric discharge machine
 
 
  Punching press
 
 
 
  Woodworking Machine
 
 
  NC drilling machine
 
 
 
  Tapping center
 
 
 
  Pallet changer
 
 
 
 
  ATC
 
 
 
 
  Wire cutter
 
 
 
  Dresser
 
 
 
Application
Accuracy Grade
     
N
H
P
S
U
  Cartesian coordinate robot
 
 
  Cylindrical coordinate robot
 
 
 
  Wire bonder
 
 
 
  Prober
 
 
 
  Electronic-Component inserter
 
 
 
  Printed-circuit-board drilling machine
 
 
  Injection-molding machine
 
 
 
  3D measuring instrument
 
 
 
  Office equipment
 
 
 
  Transfer equipment
 
 
 
  XY table
 
 
  Painting machine
 
 
 
  Welding machine
 
 
 
  Medical Equipment
 
 
 
  Digitizer
 
 
  Inspection Equipment
 
 
  N = Normal Precision H = High Precision P = Precision S = Super Precision U = Ultra Precision
Download the Technical Data Sheet
OR
Contact an Application Engineer for more info
 
 

Or Call Now
For More Information
1-888-777-1497

 
 
 

Large Printer Glides Smoothly Along PBC Linear Path

Smooth, un-interrupted precision linear motion is essential to high end printing, and PBC Linear has been maintaining these qualities since the company first began in 1982. Using PBC Linear’s versatile MT series belt-driven linear actuator and additional support from Linear Guides, part of the Profile Rail Technology (PRT) family, a well-known high-end printer manufacturer could sustain high positional accuracy over a large work envelope for their brand new poster printing system.

This new printing station spans over a 1500 mm long assembly-line resembling work area. During the typical printing process, the inversely mounted MT actuator carefully moves carriages containing the printing stock under the transverse motion of the ink jet print head for accurate, efficient, and high quality printing. However, the printing base—where the paper sits during the printing process—periodically needed mandatory cleaning and standard maintenance. This process required the 25 lb printing base to move just under three (3) feet into the purging area: a station that allows for environmentally safe disposal of printer ink. Once finished, the printer base needed to transfer back into the printing area and resume normal function.

PBC Linear recommended installing their MTB-042 linear actuator. The extruded aluminum body is protected by clear anodizing and provides a self supporting and contained linear motion system with convenient T-Slots for mounting the unit as well as accessories. The steel reinforced belt drive provides maintenance-free, accurate, smooth and quiet linear motion.  The magnetically sealed stainless steel strip cover keeps ink out and actuator particulate in.  The MTB-042 provides long-lasting precision linear motion for high-speed, high load applications—even when the actuator is inversely mounted. 

As the actuator propels and guides the print carriage.  The other side of the carriage is supported and guided by PBC Linear’s newly offered re-circulating ball linear guides (PRT) to guarantee smooth and quiet linear motion. The runner block carriages come standard with innovative ball cages to provide higher loads, less lubrication maintainance and smooth and quiet operation. An internal lubrication system promotes long product life. PBC Linear’s new linear guide eliminates moment loads applied to the actuator—creating a stable, long-lasting linear motion system.

Overall, the printer manufacturer was impressed by the performance of the combined linear system. The vital smooth guidance provided by PBC linear was exactly what the company needed for the high-end printing station. For more information on Profile Rail Technology (PRT), or Linear Actuator Technology (LAT) please call 1.800.729.9085, email to marketing@pacific-bearing.com, or visit us at one of our dedicated landing pages: LAT.pbclinear.com.

 

View our wide array of linear motion solutions
at www.PBClinear.com NOW!

 
 
PBC Linear | 6402 Rockton Road, Roscoe, IL 61073 | P. O. Box 6980, Rockford, IL 61125-6980 | Toll-Free (888) 389-6266 | Fax: (815) 389-5790

© PBC Linear - A Pacific Bearing Company | All Rights Reserved.

Round Shaft Technology | Cam Roller Technology | Integral-V Technology | Gliding Surface Technology | Linear Actuator Technology | Profile Rail Technology | Miniature Linear Actuators
SIMO Technology| PBC Linear Linear Motion Catalogs| Hevi-Rail Heavy Duty Bearings| Uni-Guide Modular Guide Systems