Bearing systems can easily be put to the test in many diverse and challenging mobile and on-vehicle applications. In the video below, we examine several types of these mobile applications including truck bed extenders, horizontal lift systems, pressure washer trailers, and more. We further examine how to solve these application challenges utilizing Cam Roller Technology (CRT), specifically focusing on Hevi-Rail® and Redi-Rail® product solutions from PBC Linear.
Hevi-Rail has several performance characteristics that make it ideal for heavy-use cases, exemplifying its linear might in motion. Some of these properties include low coefficient of friction, high load ratings, and the ability to easily roll in and out of the rail. Redi-Rail has a more moderate load capacity than Hevi-Rail, but still offers plenty of strength coupled with a higher, practical precision that is often adequate for applications not requiring the super-high precision of the common profile rail.
Together, these two CRT products from PBC Linear offer ready solutions to many mobile application challenges. Advantages for both products include high load capacities with lightweight aluminum structure, resistance to harsh conditions, and ease of installation and alignment. When designed using the proper bearing components, mobile applications can be made much safer, more reliable, and provide more flexibility and convenience to the users.
One perfect example are the truck bed extenders for pickups or other flatbed trucks. In this scenario, Hevi-Rail technology offers a low coefficient of friction that allows for a heavy item, such as a full-size tool chest, to be moved easily. Its supports horizontal and vertical motion, as well as cantilevered loads. Additionally, the clearance between the OD of the large radial roller and the profile channel allow the bearings to roll forward and backward with ease.
Some other examples of mobile and on vehicle applications that utilize Hevi-Rail and Redi-Rail products from PBC Linear are listed below.
Applications featuring Hevi-Rail's linear might in motion:
Applications featuring Redi-Rail's practical precision: