A manufacturing facility of cooling equipment boasts a 24-hour continuous operation involving two post hydraulic presses. Each press is comprised of 2-inch round shafting. This machinery operates within the foam insulating area of the plant, and therefore experiences severe contamination from the over-spray of foam.
This contamination was the main problem for the bearings and machinery. The heavy salt content in the air causes severe corrosion, and as a result, the bronze bearings and shafts would fail every 6 weeks due to contamination and the subsequent loss of lubrication.
Bronze bearings were replaced with DDS 24 Double Flange Mounts, and then modified to accept FL 32 bearings. Four sets were used per fixture.
The DDS 24 bearings have been working for two years without incident or downtime. The customer has been pleased with the extended performance of the bearings, and the ability to now produce and ship this seasonal product on time.