Linear Bearing Pillow Block Selection Criteria
Pillow blocks, as with flange mounts, are a type of mounted bearing that contains a set of mounting holes that line up perpendicular to the mounting shaft. Through these mounting holes, pillow blocks can be secured to a foundation to facilitate a rotating shaft, or part of a bearing assembly that moves along a linear shaft. PBC Linear offers three basic types of pillow blocks that utilize either sliding plain bearings, recirculating balls, or rollers where the bearing meets shaft. Which one you decide on will depend on your specific needs that are defined by careful assessment of the application and the resulting set of criteria.
We often encourage customers to apply the P.O.S.T.L.U.D.E.S acronym, which is a convenient guide to asking the right questions for determining the best product for the job. The acronym stands for Precision, Orientation, Speed, Travel, Load, Unknowns, Duty Cycle, Environment, and Safety. The sections below offer some of the P.O.S.T.L.U.D.E.S. criteria for each of the three types of pillow blocks. Additionally, this article touches on the more complicated load and orientation dynamics. Should the reader feel inclined to further investigate these helpful criteria, they may find more satisfactory bearing selection outcomes.
Pillow block construction and applications
Pillow blocks from PBC Linear are constructed with an aluminum alloy housing and are offered in many sizes as well as metric or imperial configurations. Certain combinations of housing type, bearing type, and shafting will provide the best pillow block bearing for a given application or condition. For example, all three types can be purchased in the open format, which accommodates support rails for shafts requiring longer or more rigid travel. Plain and recirculating ball bearings also have closed designs for use in end-supported applications.
Standard plain and ball type pillow blocks from PBC Linear combine a self-aligning housing with either a Simplicity® plain bearing or recirculating ball bearing. This self-aligning crown allows up to 1/2 degree of mis-alignment in the application, making it helpful in avoiding binding caused by misalignment. For single shaft applications demanding more rigidity, both plain and ball type bearings can be purchased with a straight bore ID in the housing. The basic rundown and P.O.S.T.L.U.D.E.S. criteria on our three types of pillow blocks are as follows:
Plain type pillow blocks from PBC Linear combine a standard Simplicity® plain bearing with a self-aligning aluminum housing. They feature a self-lubricating liner that offers quiet operation, low maintenance, and lower overall costs.
- Precision: Good but less than ball bearings, no adjustable preload
- Orientation: All
- Speed: Higher speeds than ball bearings
- Travel: Good in short stroke applications
- Loads: Higher load capacities than standard ball bearings
- Unknowns: Application variables will factor into dynamic load capacities
- Duty cycle: Low due to high coefficient of friction
- Environment: Good in harsh environments including caustic washdown
Find more info on plain bearings with our blogs Simplicity - Designed to Last and Design Factors for Simplicity Bearings, or go to our products page for Plain Bearing Pillow Blocks.
Ball type pillow blocks utilize similar housings as plain bearings but instead embed recirculating ball bearings that provide the contact between housing and shaft. Ball-type pillow blocks from PBC Linear have standardized dimensions that provide ease of assembly and accurate replacement.
- Precision: Highest, adjustable preload for high rigidity
- Orientation: All
- Speed: Lower max speed than plain or roller type bearings
- Travel: Good in longer strokes
- Loads: Limited due to point-to-point contact of balls to shaft
- Duty cycle: Good in continous motion because of low coefficient of friction
- Environment: Poor resistance to corrosion/contamination
Visit our products page for more on
Ball-type Pillow Blocks, or compare plain and ball-type bearings in the white paper
Designing Weight Stack and Fitness Equipment Applications.
Roller type pillow blocks are quick, accurate, and steady through the toughest conditions. They employ either a single set of three rollers (one on top, two on the sides with an adjustable eccentric cam) or a double set of six. The twin model provides a larger base with greater stability. All sizes offer exceptional smooth travel as well as a floating pillow block option that reduces alignment issues and installation costs:
- Precision: Low to medium applications
- Orientation: Horizontal applications
- Speed: High speeds up to 25 ft/sec
- Travel: Long travel with low vibration and ease over joined shafts
- Loads: High dynamic load capacity
- Duty cycle: Rollers provide low coefficient of friction resulting in less heat and wear
- Environment: Good contaminant resistance
Find more info by viewing our blog/videos for Overview of the Roller Pillow Block, Roller Bearing Pillow Block Adjustment or visit our products page for Roller Pillow Blocks.
Establish your load needs
Load refers to the forces acting upon a system and includes either static, dynamic, or impact components. A static load condition occurs when the system is fully loaded and at rest, and is the easiest condition to define. Dynamic loads, which look to quantify forces applied during motion, better reflect the actual loads experienced by the bearing during machine operation. This is important because when bearing systems are in motion, they need to contend with a larger set of variables that can affect overall performance. This set of variables makes calculating dynamic loads trickier, but not impossible. For example, plain bearings can offer static loads up to 20-times higher than ball bearings. However, in dynamic situations, the larger surface area of plain bearings is more sensitive to variations, and subsequently require additional calculations such as PV value: where P= Pressure (applied load divided by reflected surface area), and V = Surface Speed. To learn more about how to calculate the PV value, please view our blog: Calculating PV for Plain Bearings.
This dynamic load chart offers an example of the different dynamic load ratings using the example of a 1-inch shaft diameter. As is illustrated, the double and twin pillow blocks initially offer the most load capacity for pillow block configurations, while plain bearings are dependent on the PV value derived from the specific application.
Depending on the type of application, moment loads should be factored into the decision on bearing selection. Moment loads apply a force that causes a bearing to rotate about a specific point or axis, and will increase relative to the distance of the load from the bearing’s center line. Moment load forces are defined as pitch, yaw, or rotational movement. Ball bearings offer modest resistance to moment loads, but can sustain increased wear if loads are too high. Plain bearings are limited to the 2:1 ratio often related to cantilevered loads. (Learn more about the 2:1 ratio with our white paper Demystifying the 2-1 Ratio and Stick-Slip Phenomenon). Roller pillow blocks are less resilient to moment loads because the cantilever or moments will load the side rollers and cause premature failure.
Orientation can affect load capacity and performance
Load orientation and its effect on load capacities in Simplicity bearings. The orientation, or how a system is mounted, can affect the load capacity and consequently the performance of a pillow block. Orientation can be defined as horizontal, vertical, side, inverted, angled, etc. Closed versions of Simplicity plain and ball-type bearings can operate in any orientation. With open bearings, load capacities will vary depending on the orientation in which they are being used. The load orientation graphic demostrates how the orientation will affect Simplicity bearings' load capacity.
Roller pillow blocks are best suited for horizontal motion in an upright position, and those interested in implementing them in vertical and moment load applications should consult our application engineers for assistance.
Discover your ideal linear motion solution: